EN1992-4 compliant verification of the anchor plate bending stiffness - the new solution in the free PROFIS Engineering Standard
With the inclusion of EN 1992-4 in the MVV-TB in January 2021, anchor design has become more important. The rules and regulations for successful and safe anchor design have also come to the fore. An important component on which these rules and regulations are based is the approach of a linear load distribution based on a rigid anchor plate or the approach of the actual anchor loads. This simplified concept is difficult to verify and often does not correspond to reality. We would like to show you how you can achieve a fast, transparent, secure and EN 1992-4 compliant solution with our free software solution PROFIS Engineering.