Update of quantity
Please note, the order volume has been updated. This is due to package and minimum order quantities.
Please note, the order volume has been updated to. This is due to package and minimum order quantities.
Pipes can expand and contract for two reasons:
In both these cases pipes should not be fixed to brackets, but instead should have the freedom to move longitudinally.
Use sliders to allow the expansion of the pipe without stressing the channel system or the pipe ring. Use fixed points combined with expansion compensators to make sure there’s an equal distribution of the movements of the pipe and to absorb additional forces that are generated.
QUICK LINKS
To see account specific prices and content, please choose appropriate account.